AnsweredAssumed Answered

USB Virtual COM Port driver code

Question asked by norair.jp on Jan 15, 2012
Latest reply on Mar 15, 2012 by sumpner.paul
Hi: the USB functionality on the STM32 is great, but it is not really deployable for USB-serial given that the only Virtual COM (or Virtual TTY) driver is for Windows.  For dev-kits, windows is OK.  For actual products, it is not OK anymore.

I am going to write open source drivers for Linux/POSIX and Mac+iOS.  I am requesting ST to release the source for the Windows driver, because this will mean that the Linux driver is as close to the windows driver as possible, and it will also make it easier & faster to develop.

Outcomes