AnsweredAssumed Answered

FTP Client on STM32

Question asked by mjbcswitzerland on Jan 7, 2012
Latest reply on Jan 9, 2012 by AMSN
Hi All

The following new video shows a demonstration of embedded FTP client operation in the uTasker project: http://youtu.be/sZOCFLDfGTk It is not shown running on an STM32 board in the demo but it is now included in the uTasker STM32 project as detailed here: http://www.utasker.com/forum/index.php?topic=1697.0

It is therefore operational on STM32F1, STM32F2 and STM32F4 evaluation boards using GCC, Rowley Crossworks, ATOLLIC TrueStudio, IAR or Keil uVision, as well as in real-time simulation in VisualStudio 6 or VisualStudio 20xx.

The FTP client user's manual is available at http://www.utasker.com/docs/uTasker/uTaskerFTP_client.pdf

Regards

Mark

Outcomes