AnsweredAssumed Answered

Pb with FreeRTOS and USB

Question asked by lasserre.serge on Jan 5, 2012
Latest reply on Jan 8, 2012 by FreeRTOS.org
Hello,
We are working on the STM3220-G Evaluation Board.
We are using IAR compiler [V6.2] and running a test application with FreeRTOS [7.0.2] and the STM32_F105-07_F2xx_USB-Host-Device_Lib_V2.0.0
The USB is used as Virtual Com Port.
The USB alone works correctly.
The FreRTOS alone works correctly (with only one task).

But when I put USB with FreeRTOS, I have systematically a crash on the IAR environnement (don't answer), I must close the environnment
Have someone already have this kind of problem, please?

Regards

Outcomes