AnsweredAssumed Answered

Problem with programming protected device

Question asked by xadamus on Dec 19, 2011
Latest reply on Jan 2, 2012 by Clive One
Hello. I have problem with upgrading program in my own bootloader.

When procesor is not read-out protected, everything is going ok (verify says ok).
Problem occurs when I set <Read-Out Protection> in RFlasher7 (using Ride7 and RLink programmer). Internal program is erased ok (mass erase) but it stops after first full word programming command (flash controller returns FLASH_FLAG_BANK1_WRPRTERR). In Option Bytes non of the WRP0-WRP3 is set (all have 0xFF).
Where is a problem ?


And one more guestion: Are option bytes erased during mass erase command ? Should I set up readOutProtection again after mass erase command ?

Outcomes