AnsweredAssumed Answered

PM6680A based project simulation in eDesign Studio

Question asked by imberti.mirko on Mar 27, 2014
Latest reply on Mar 27, 2014 by PALANO Carmelo Marcello
1) After saving either locally or remotely the project, I can't find anymore my database added components. Could it be wanted or a bug?
2) PSpice export option is grayed, is it because ST PSpice Project Export Manager isn't installed yet, or the PM6680A PSpice export is not supported yet?
3)The resistor divider proposed for undervoltage function looks unrealistic (100K hr, 1.47M lr for a 19 to 30V input range)...
Thanks in advance

Outcomes