AnsweredAssumed Answered

Backup register not working on STM32F105RC

Question asked by pande.vedprakash on Sep 30, 2011
Latest reply on Oct 14, 2011 by pande.vedprakash

I am using STM32F105RC microcontroller on a custom designed board, the microcontroller runs at 72MHz, no crystal (& its decoupling caps) is connected for RTC, CR2032 3V battery is connected to Vbat directly (no other circuit like diode between Vbat & Vdd is present). I am using IAR embedded workbench.

The code is as follows:

#include "stm32f10x.h"

#include <intrinsics.h>

#include "global.h"

#include "stm32f10x_rtc.h"

#include "stm32f10x_bkp.h"

 

int main()

{

    GPIO_InitTypeDef GPIO_InitStructure;

    SystemInit();

     

#ifndef  EMB_FLASH

  /* Set the Vector Table base location at 0x20000000 */

  NVIC_SetVectorTable(NVIC_VectTab_RAM, 0x0);

#else  /* VECT_TAB_FLASH  */

  /* Set the Vector Table base location at 0x08000000 */

  NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x1000);

#endif

  NVIC_PriorityGroupConfig(NVIC_PriorityGroup_4);

   

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA |        

                         RCC_APB2Periph_GPIOB |

                         RCC_APB2Periph_GPIOC |

                         RCC_APB2Periph_GPIOD,

                         ENABLE);

  RCC_APB2PeriphResetCmd(RCC_APB2Periph_GPIOA |

                         RCC_APB2Periph_GPIOB |

                         RCC_APB2Periph_GPIOC |

                         RCC_APB2Periph_GPIOD,

                         DISABLE);

 

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;        

 

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_4;

  GPIO_Init(GPIOA, &GPIO_InitStructure);

   

  GPIO_WriteBit(GPIOA,GPIO_Pin_0 ,Bit_RESET);  

 

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR | RCC_APB1Periph_BKP, ENABLE); 

  PWR_BackupAccessCmd(ENABLE); 

/*  if (BKP_ReadBackupRegister(BKP_DR1) != 0xA5A5) 

  {

    BKP_DeInit();

    BKP_WriteBackupRegister(BKP_DR1, 0xA5A5);

  }*/

  while(1)

  {

      if (BKP_ReadBackupRegister(BKP_DR1) == 0xA5A5)

      {

          GPIO_WriteBit(GPIOA,GPIO_Pin_0 ,Bit_SET);   

      }

  }

}

I test it as follows:

When the commented code is uncommented (the code beginning with if (BKP_ReadBackupRegister(BKP_DR1) != 0xA5A5)), then program is compiled & run in debug mode, the LED connected to GPIO_Pin_0 glows. When the board is not powered off, code is commented again (as shown above) & code is run in debug mode, the LED still glows. But if the board is powered off & turned on again, the LED does not glow. It seems the backup registers are not working.

Can you please help me to solve this problem?

Thanks in advance!

Outcomes