AnsweredAssumed Answered

stm32F205 and usb

Question asked by y.micha3 on Sep 19, 2011
Latest reply on Jan 13, 2012 by jlj
Hi everyone,
I want to use usb in stm32f205
In documentation http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/DATASHEET/CD00237391.pdf on page 12 it is written that this microcontroler has only OTG_HS/OTG_FS , but on page http://www.st.com/internet/mcu/product/250189.jsp its written that it has:
       
  • USB 2.0 full-speed device/host/OTG controller with on-chip PHY
       
  • USB 2.0 high-speed/full-speed device/host/OTG controller with dedicated DMA, on-chip full-speed PHY and ULPI
If there is only OTG_HS/OTG_FS  than  which pin should I use to for OTG_FS:

PA12 and PA11
or
PB13 PB14?

Outcomes