AnsweredAssumed Answered

The dreaded handler hardfault on new build chain

Question asked by loerchner.axel on Aug 23, 2011
Latest reply on Mar 23, 2012 by ramirez_correa.steph
Greetings,
I am new to the STM32 family of devices and am trying to build for the FUTURELEC STM32 Stamp Board, which has on it the stm32f103ret6 processor. Link:

http://www.futurlec.com/ET-STM32_Stamp.shtml

I am able to build and flash the binary image, but immediately receive the HANDLER HARDFAULT message upon running the code. I have futzed around with this for about a week and pretty well out of ideas. Any help would be appreciated.

I am building on UBUNTU 10.04, using the latest CodeSourcery release, and the latest (3.5.0)release of the ST libraries. For flashing I use the Olimex ARM-USB-TINY with OpenOCD.

I set up the project environment using the guide supplied on this page, and followed the instructions to the letter:

http://stm32.spacevs.com/index.php?option=com_content&view=featured&Itemid=101

This guide uses the 3.3.0 version of the libraries. The necessary changes were made to reference the current 3.5.0 libraries.

Compiler output:

-----------------------------------------------------------------------------------
/usr/bin/make -C libs libs
make[1]: Entering directory `/home/.../MotionController_5_Phase_CORTEX/libs'
Building libstm32.a ...done.
make[1]: Leaving directory `/home/.../MotionController_5_Phase_CORTEX/libs'
/usr/bin/make -C src src
make[1]: Entering directory `/home/.../MotionController_5_Phase_CORTEX/src'
make[1]: Nothing to be done for `src'.
make[1]: Leaving directory `/home/.../MotionController_5_Phase_CORTEX/src'
arm-none-eabi-gcc -o main.elf -O3 -g -mcpu=cortex-m3 -mthumb -fno-exceptions -ffunction-sections -fdata-sections -L/home/.../MotionController_5_Phase_CORTEX/libs -nostartfiles -Wl,--gc-sections,-Tlinker.ld -Wl,--whole-archive src/app.a -Wl,--no-whole-archive -lm -lstm32
arm-none-eabi-objcopy -O ihex    main.elf main.hex
arm-none-eabi-objcopy -O binary main.elf main.bin


I replaced the path between "home/" and "/MotionController_5_Phase_CORTEX" with "..." for this email. Output of the flash operation and execution is as follows:

>
> flash write_image erase /home/.../MotionController_5_Phase_CORTEX/main.bin 0x8000000
auto erase enabled
wrote 1352 byte from file /home/.../MotionController_5_Phase_CORTEX/main.bin in 0.272857s (4.838844 kb/s)
>
> reset run                                                                                                                                                      
JTAG tap: stm32.cpu tap/device found: 0x3ba00477 (mfg: 0x23b, part: 0xba00, ver: 0x3)
JTAG tap: stm32.bs tap/device found: 0x06414041 (mfg: 0x020, part: 0x6414, ver: 0x0)
target state: halted
target halted due to breakpoint, current mode: Handler HardFault
xPSR: 0x00000003 pc: 0x20000004 msp: 0x20004fe0
>

Register listing is:

> reg
===== arm v7m registers
(0) r0 (/32): 0x20000578
(1) r1 (/32): 0x08000548
(2) r2 (/32): 0x00000000
(3) r3 (/32): 0x00000023
(4) r4 (/32): 0x40022010
(5) r5 (/32): 0x4002200C
(6) r6 (/32): 0xE000E000
(7) r7 (/32): 0x20004FE0
(8) r8 (/32): 0xFFDEFFFE
(9) r9 (/32): 0xFFEFED79
(10) r10 (/32): 0xF07AC9EE
(11) r11 (/32): 0x01001EB3
(12) r12 (/32): 0xFF7FDFFF
(13) sp (/32): 0x20004FE0
(14) lr (/32): 0xFFFFFFF9
(15) pc (/32): 0x20000004
(16) xPSR (/32): 0x00000003
(17) msp (/32): 0x20004FE0
(18) psp (/32): 0x7B621F90
(19) primask (/1): 0x00
(20) basepri (/8): 0x00
(21) faultmask (/1): 0x00
(22) control (/2): 0x00
>

Any ideas what I'm doing wrong?

Thanks in advance.

Outcomes