AnsweredAssumed Answered

CAN testing in nomal mode

Question asked by rose abraham on Jul 29, 2011
Latest reply on Jul 29, 2011 by STOne-32
I have been testing CAN on a board using stm32f107vc cpu.I have done the testing first using the example code from st site where CAN will communicate in loop-back mode. That was working fine. I tailored the code to test CAN in normal mode. For this i have connected two custom boards back to back.The test failed as the received message is not matching to the transmitted one. But while doing probing with an oscilloscope both the tranmitted and the received message are perfectly matching. Please help ...any suggetions would be highly appreciated.

Outcomes