AnsweredAssumed Answered

Using STM32F10x USB device with Windows Vista or Windows 7

Question asked by moardy on Jul 21, 2011
Latest reply on May 30, 2013 by Clive One
Hello,

we are using  an STM32F105 as USB device in conjunction with a special
configuration program, that runs on a PC.
If we use a PC with Windows XP, the USB driver is automatically
installed and all works fine.
But if we try the same with a PC running Windows Vista or 7, a driver is NOT
automatically installed and the device is marked as 'not working'.
The only way to avoid this, is a prior installation of the 'dfuSe' package.
After installation of this package, the USB connection works, if you connect
the MCU and the PC.

Is there any other way (for driver installation), without prior installation of
the 'dfuSe' package
?

Thanks for all answers !

Regards

moardy


Outcomes