AnsweredAssumed Answered

Core cm3

Question asked by jourdan.cyril on Jun 21, 2011
Latest reply on Jul 4, 2011 by rosarium
extern uint32_t __get_PSP(void);
Hello,
When I compile an example, I have all these errors, they said incomptabile declaration for all the folowing list:

extern void __set_PSP(uint32_t topOfProcStack);
extern uint32_t __get_MSP(void);
extern void __set_MSP(uint32_t topOfMainStack);
extern uint32_t __REV16(uint16_t value);
extern uint32_t __RBIT(uint32_t value);
extern uint32_t __STREXB(uint8_t value, uint8_t *addr);
extern uint32_t __STREXH(uint16_t value, uint16_t *addr);


For solving this problem I set it as note with "//" (ctrl+K)

Is it the good way to do ?
What does it change?

Thanks

Outcomes