AnsweredAssumed Answered

STM3210C_EVAL and LwIP implementation example (AN3102)

Question asked by romain.rimboud on Jun 13, 2011
Latest reply on Jun 13, 2011 by Clive One
Hi all.

I tried to use the AN3102 example, which enable to implement the LwIP Ethernet stack on mu dedicated STM3210C_EVAL, composed of an STM32F107 µC.

However, when I link it to the network or directly to my computer, I can't run the telnet or http examples. I tried to "ping" the board but the command guest display "Hardware Error".
All addresses (MAC, PHY and IP) seem to be correctly initialized and jumpers are correctly placed on the board (as is explained in the Application Note)

So I wish to know where does the problem come from, and which are the ways can I explore in the code to resolve it.

Thanks you all in advance!

Outcomes