AnsweredAssumed Answered

Read pressure sensor with I2C in master receiver mode

Question asked by gillespie.philip on Jun 8, 2011
Hi All,

Need some advise here with I2C.  I'm trying to use I2C in master receiver mode to read two bytes of data out of a pressure sensor.  The required command sequence is pg 8 of attached data sheet.

Here is the code:

       GPIO_InitTypeDef  GPIO_InitStructure;

       /* SDA */
      GPIO_InitStructure.GPIO_Pin =     GPIO_Pin_7;
      GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
      GPIO_InitStructure.GPIO_Mode =   GPIO_Mode_AF_OD;
      GPIO_Init(GPIOB, &GPIO_InitStructure);

      GPIO_InitStructure.GPIO_Pin       =   GPIO_Pin_6;
      GPIO_InitStructure.GPIO_Speed   =  GPIO_Speed_50MHz;          
      GPIO_InitStructure.GPIO_Mode    =  GPIO_Mode_AF_OD;              
      GPIO_Init(GPIOB, &GPIO_InitStructure);

       I2C_InitTypeDef  I2C_InitStructure;

     /* I2C configuration */
     I2C_InitStructure.I2C_Mode = I2C_Mode_I2C;
     I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2;
     I2C_InitStructure.I2C_OwnAddress1 = I2C1_SLAVE_ADDRESS7;
     I2C_InitStructure.I2C_Ack = I2C_Ack_Enable;
     I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;
     I2C_InitStructure.I2C_ClockSpeed = I2C_Speed;
     I2C_Cmd(I2C1, ENABLE);
     I2C_Init(I2C1, &I2C_InitStructure);


        int sensor_data[2];
        sensor_data[0] = 0x00;
        sensor_data[1] = 0x00;

        /* Enable I2C1 acknowledgement if it is already disabled by other function */
        I2C_AcknowledgeConfig(I2C1, ENABLE);

        /* While the bus is busy */
        while(I2C_GetFlagStatus(I2C1, I2C_FLAG_BUSY));

        /*----- Transmission Phase -----*/
        /* Send START condition */
        I2C_GenerateSTART(I2C1, ENABLE);

        /* Test on EV5 and clear it */
        while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT));
                       
        /* Send sensor address */
        I2C_SendData(I2C1,0xF1);       

        /* Test on EV6 and clear it */
        while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_RECEIVER_MODE_SELECTED));
                        
        /* Read a byte from the sensor*/
          sensor_data[0] = I2C_ReceiveData(I2C1);
       
        /* Test on EV7 and clear it */
        while(I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_RECEIVED));
       
        sensor_data[1] = I2C_ReceiveData(I2C1);
       
        /* Test on EV7 and clear it */
        while(I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_RECEIVED));
           
        /* Send I2C1 STOP Condition */
        I2C_GenerateSTOP(I2C1, ENABLE);


After i send out the address of the sensor, i'm seeing (on the scope) two byte of data with 18 clock cycles.  I assumed this data is only read out using I2C_ReceiveData? Also is a NACK command required before stop commmand?
Any suggestions about what I'm not doing correctly would be greatly appreciated.

--
Thanks  

Attachments

Outcomes