AnsweredAssumed Answered

STM32F479- AUDIO CODEC PROBLEM

Question asked by pk.srividya on Nov 16, 2016
Latest reply on Nov 30, 2016 by ForumSTM32.ForumSTM3
Hi,
I am trying to capture the audio data into a .bin or .wav file with the header.
To capture the data into the file, using emmc for storage of file and fatfs for storing into the file. The part number used for microphone is ics43432.

Capture of receiving the mic data is done using hal_i2s_receive_dma.
While debugging, the execution of DMA_START_IT is successful giving the status at the end. Dma interrupts are obtained and print statements inside the handler are also being seen on the terminal.

For the DMA transfer i'm using a transfer_complete_callback(xfercpltcallback-a function pointer).
In the handler, the execution has to shift automatically from handler to the function(I2S_DMARxCplt) pointed by the pointer. At this point the execution is not entering the function.

Are there any issues in the code enclosed. Kindly let me know. It would be of great help if you could help me solve the problem.


/**
  * @brief  Handles DMA interrupt request.
  * @param  hdma: pointer to a DMA_HandleTypeDef structure that contains
  *               the configuration information for the specified DMA Stream.  
  * @retval None
  */
void HAL_DMA_IRQHandler(DMA_HandleTypeDef *hdma)
{
  uint32_t tmpisr;
  __IO uint32_t count = 0;
  uint32_t timeout = SystemCoreClock / 9600;

  /* calculate DMA base and stream number */
  DMA_Base_Registers *regs = (DMA_Base_Registers *)hdma->StreamBaseAddress;

  tmpisr = regs->ISR;

  /* Transfer Error Interrupt management ***************************************/
  if ((tmpisr & (DMA_FLAG_TEIF0_4 << hdma->StreamIndex)) != RESET)
  {
    if(__HAL_DMA_GET_IT_SOURCE(hdma, DMA_IT_TE) != RESET)
    {
      /* Disable the transfer error interrupt */
      hdma->Instance->CR  &= ~(DMA_IT_TE);
      
      /* Clear the transfer error flag */
      regs->IFCR = DMA_FLAG_TEIF0_4 << hdma->StreamIndex;
      
      /* Update error code */
      hdma->ErrorCode |= HAL_DMA_ERROR_TE;
    }
  }
  /* FIFO Error Interrupt management ******************************************/
  if ((tmpisr & (DMA_FLAG_FEIF0_4 << hdma->StreamIndex)) != RESET)
  {
    if(__HAL_DMA_GET_IT_SOURCE(hdma, DMA_IT_FE) != RESET)
    {
      /* Clear the FIFO error flag */
      regs->IFCR = DMA_FLAG_FEIF0_4 << hdma->StreamIndex;

      /* Update error code */
      hdma->ErrorCode |= HAL_DMA_ERROR_FE;
    }
  }
  /* Direct Mode Error Interrupt management ***********************************/
  if ((tmpisr & (DMA_FLAG_DMEIF0_4 << hdma->StreamIndex)) != RESET)
  {
    if(__HAL_DMA_GET_IT_SOURCE(hdma, DMA_IT_DME) != RESET)
    {
      /* Clear the direct mode error flag */
      regs->IFCR = DMA_FLAG_DMEIF0_4 << hdma->StreamIndex;

      /* Update error code */
      hdma->ErrorCode |= HAL_DMA_ERROR_DME;
    }
  }
  /* Half Transfer Complete Interrupt management ******************************/
  if ((tmpisr & (DMA_FLAG_HTIF0_4 << hdma->StreamIndex)) != RESET)
  {
    if(__HAL_DMA_GET_IT_SOURCE(hdma, DMA_IT_HT) != RESET)
    {
      /* Clear the half transfer complete flag */
      regs->IFCR = DMA_FLAG_HTIF0_4 << hdma->StreamIndex;
      
      /* Multi_Buffering mode enabled */
      if(((hdma->Instance->CR) & (uint32_t)(DMA_SxCR_DBM)) != RESET)
      {
        /* Current memory buffer used is Memory 0 */
        if((hdma->Instance->CR & DMA_SxCR_CT) == RESET)
        {
          if(hdma->XferHalfCpltCallback != NULL)
          {
            /* Half transfer callback */
            hdma->XferHalfCpltCallback(hdma);
          }
        }
        /* Current memory buffer used is Memory 1 */
        else
        {
          if(hdma->XferM1HalfCpltCallback != NULL)
          {
            /* Half transfer callback */
            hdma->XferM1HalfCpltCallback(hdma);
          }
        }
      }
      else
      {
        /* Disable the half transfer interrupt if the DMA mode is not CIRCULAR */
        if((hdma->Instance->CR & DMA_SxCR_CIRC) == RESET)
        {
          /* Disable the half transfer interrupt */
          hdma->Instance->CR  &= ~(DMA_IT_HT);
        }
        
        if(hdma->XferHalfCpltCallback != NULL)
        {
          /* Half transfer callback */
          hdma->XferHalfCpltCallback(hdma);
        }
      }
    }
  }
  /* Transfer Complete Interrupt management ***********************************/
  if ((tmpisr & (DMA_FLAG_TCIF0_4 << hdma->StreamIndex)) != RESET)
  {
    if(__HAL_DMA_GET_IT_SOURCE(hdma, DMA_IT_TC) != RESET)
    {
      /* Clear the transfer complete flag */
      regs->IFCR = DMA_FLAG_TCIF0_4 << hdma->StreamIndex;
      
      if(HAL_DMA_STATE_ABORT == hdma->State)
      {
        /* Disable all the transfer interrupts */
        hdma->Instance->CR  &= ~(DMA_IT_TC | DMA_IT_TE | DMA_IT_DME);
        hdma->Instance->FCR &= ~(DMA_IT_FE);
        
        if((hdma->XferHalfCpltCallback != NULL) || (hdma->XferM1HalfCpltCallback != NULL))
        {
          hdma->Instance->CR  &= ~(DMA_IT_HT);
        }

        /* Clear all interrupt flags at correct offset within the register */
        regs->IFCR = 0x3FU << hdma->StreamIndex;

        /* Process Unlocked */
        __HAL_UNLOCK(hdma);

        /* Change the DMA state */
        hdma->State = HAL_DMA_STATE_READY;

        if(hdma->XferAbortCallback != NULL)
        {
          hdma->XferAbortCallback(hdma);
        }
        return;
      }

      if(((hdma->Instance->CR) & (uint32_t)(DMA_SxCR_DBM)) != RESET)
      {
        /* Current memory buffer used is Memory 0 */
        if((hdma->Instance->CR & DMA_SxCR_CT) == RESET)
        {
          if(hdma->XferM1CpltCallback != NULL)
          {
            /* Transfer complete Callback for memory1 */
            hdma->XferM1CpltCallback(hdma);
          }
        }
        /* Current memory buffer used is Memory 1 */
        else
        {
          if(hdma->XferCpltCallback != NULL)
          {
            /* Transfer complete Callback for memory0 */
            hdma->XferCpltCallback(hdma);
          }
        }
      }
      /* Disable the transfer complete interrupt if the DMA mode is not CIRCULAR */
      else
      {
        if((hdma->Instance->CR & DMA_SxCR_CIRC) == RESET)
        {
          /* Disable the transfer complete interrupt */
          hdma->Instance->CR  &= ~(DMA_IT_TC);

          /* Process Unlocked */
          __HAL_UNLOCK(hdma);

          /* Change the DMA state */
          hdma->State = HAL_DMA_STATE_READY;
        }

        if(hdma->XferCpltCallback != NULL)
        {
          /* Transfer complete callback */
          hdma->XferCpltCallback(hdma);
        }
      }
    }
  }
 
  /* manage error case */
  if(hdma->ErrorCode != HAL_DMA_ERROR_NONE)
  {
    if((hdma->ErrorCode & HAL_DMA_ERROR_TE) != RESET)
    {
      hdma->State = HAL_DMA_STATE_ABORT;

      /* Disable the stream */
      __HAL_DMA_DISABLE(hdma);

      do
      {
        if (++count > timeout)
        {
          break;
        }
      }
      while((hdma->Instance->CR & DMA_SxCR_EN) != RESET);

      /* Process Unlocked */
      __HAL_UNLOCK(hdma);

      /* Change the DMA state */
      hdma->State = HAL_DMA_STATE_READY;
    }

    if(hdma->XferErrorCallback != NULL)
    {
      /* Transfer error callback */
      hdma->XferErrorCallback(hdma);//execution stops here
    }
  }
}


/**

 ===============================================================================
                  ##### How to use this driver #####
 ===============================================================================
 [..]
    The I2S HAL driver can be used as follow:
    
    (#) Declare a I2S_HandleTypeDef handle structure.
    (#) Initialize the I2S low level resources by implement the HAL_I2S_MspInit() API:
        (##) Enable the SPIx interface clock.                      
        (##) I2S pins configuration:
            (+++) Enable the clock for the I2S GPIOs.
            (+++) Configure these I2S pins as alternate function pull-up.
        (##) NVIC configuration if you need to use interrupt process (HAL_I2S_Transmit_IT()
             and HAL_I2S_Receive_IT() APIs).
            (+++) Configure the I2Sx interrupt priority.
            (+++) Enable the NVIC I2S IRQ handle.
        (##) DMA Configuration if you need to use DMA process (HAL_I2S_Transmit_DMA()
             and HAL_I2S_Receive_DMA() APIs:
            (+++) Declare a DMA handle structure for the Tx/Rx stream.
            (+++) Enable the DMAx interface clock.
            (+++) Configure the declared DMA handle structure with the required Tx/Rx parameters.
            (+++) Configure the DMA Tx/Rx Stream.
            (+++) Associate the initialized DMA handle to the I2S DMA Tx/Rx handle.
            (+++) Configure the priority and enable the NVIC for the transfer complete interrupt on the
                DMA Tx/Rx Stream.
 
   (#) Program the Mode, Standard, Data Format, MCLK Output, Audio frequency and Polarity
       using HAL_I2S_Init() function.

   -@- The specific I2S interrupts (Transmission complete interrupt,
       RXNE interrupt and Error Interrupts) will be managed using the macros
       __I2S_ENABLE_IT() and __I2S_DISABLE_IT() inside the transmit and receive process.
   -@- Make sure that either:
        (+@) I2S PLL is configured or
        (+@) External clock source is configured after setting correctly
             the define constant EXTERNAL_CLOCK_VALUE in the stm32f4xx_hal_conf.h file.
             
   (#) Three operation modes are available within this driver :
 
   *** Polling mode IO operation ***
   =================================
   [..]    
     (+) Send an amount of data in blocking mode using HAL_I2S_Transmit()
     (+) Receive an amount of data in blocking mode using HAL_I2S_Receive()
   
   *** Interrupt mode IO operation ***
   ===================================
   [..]    
     (+) Send an amount of data in non blocking mode using HAL_I2S_Transmit_IT()
     (+) At transmission end of half transfer HAL_I2S_TxHalfCpltCallback is executed and user can
         add his own code by customization of function pointer HAL_I2S_TxHalfCpltCallback
     (+) At transmission end of transfer HAL_I2S_TxCpltCallback is executed and user can
         add his own code by customization of function pointer HAL_I2S_TxCpltCallback
     (+) Receive an amount of data in non blocking mode using HAL_I2S_Receive_IT()
     (+) At reception end of half transfer HAL_I2S_RxHalfCpltCallback is executed and user can
         add his own code by customization of function pointer HAL_I2S_RxHalfCpltCallback
     (+) At reception end of transfer HAL_I2S_RxCpltCallback is executed and user can
         add his own code by customization of function pointer HAL_I2S_RxCpltCallback
     (+) In case of transfer Error, HAL_I2S_ErrorCallback() function is executed and user can
         add his own code by customization of function pointer HAL_I2S_ErrorCallback

   *** DMA mode IO operation ***
   ==============================
   [..]
     (+) Send an amount of data in non blocking mode (DMA) using HAL_I2S_Transmit_DMA()
     (+) At transmission end of half transfer HAL_I2S_TxHalfCpltCallback is executed and user can
         add his own code by customization of function pointer HAL_I2S_TxHalfCpltCallback
     (+) At transmission end of transfer HAL_I2S_TxCpltCallback is executed and user can
         add his own code by customization of function pointer HAL_I2S_TxCpltCallback
     (+) Receive an amount of data in non blocking mode (DMA) using HAL_I2S_Receive_DMA()
     (+) At reception end of half transfer HAL_I2S_RxHalfCpltCallback is executed and user can
         add his own code by customization of function pointer HAL_I2S_RxHalfCpltCallback
     (+) At reception end of transfer HAL_I2S_RxCpltCallback is executed and user can
         add his own code by customization of function pointer HAL_I2S_RxCpltCallback
     (+) In case of transfer Error, HAL_I2S_ErrorCallback() function is executed and user can
         add his own code by customization of function pointer HAL_I2S_ErrorCallback
     (+) Pause the DMA Transfer using HAL_I2S_DMAPause()
     (+) Resume the DMA Transfer using HAL_I2S_DMAResume()
     (+) Stop the DMA Transfer using HAL_I2S_DMAStop()

   *** I2S HAL driver macros list ***
   =============================================
   [..]
     Below the list of most used macros in USART HAL driver.
       
      (+) __HAL_I2S_ENABLE: Enable the specified SPI peripheral (in I2S mode)
      (+) __HAL_I2S_DISABLE: Disable the specified SPI peripheral (in I2S mode)
      (+) __HAL_I2S_ENABLE_IT : Enable the specified I2S interrupts
      (+) __HAL_I2S_DISABLE_IT : Disable the specified I2S interrupts
      (+) __HAL_I2S_GET_FLAG: Check whether the specified I2S flag is set or not

    [..]
      (@) You can refer to the I2S HAL driver header file for more useful macros

  @endverbatim
  ******************************************************************************
  * @attention
  *
  * <h2><center>&copy; COPYRIGHT(c) 2016 STMicroelectronics</center></h2>
  *
  * Redistribution and use in source and binary forms, with or without modification,
  * are permitted provided that the following conditions are met:
  *   1. Redistributions of source code must retain the above copyright notice,
  *      this list of conditions and the following disclaimer.
  *   2. Redistributions in binary form must reproduce the above copyright notice,
  *      this list of conditions and the following disclaimer in the documentation
  *      and/or other materials provided with the distribution.
  *   3. Neither the name of STMicroelectronics nor the names of its contributors
  *      may be used to endorse or promote products derived from this software
  *      without specific prior written permission.
  *
  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
  * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE
  * DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE
  * FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL
  * DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR
  * SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER
  * CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
  * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
  *
  ******************************************************************************
  */

/* Includes ------------------------------------------------------------------*/
#include "stm32f4xx_hal.h"

/** @addtogroup STM32F4xx_HAL_Driver
  * @{
  */

/** @defgroup I2S I2S
  * @brief I2S HAL module driver
  * @{
  */

#ifdef HAL_I2S_MODULE_ENABLED

/* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*/
/* Private macro -------------------------------------------------------------*/
/* Private variables ---------------------------------------------------------*/
/* Private function prototypes -----------------------------------------------*/
/** @addtogroup I2S_Private_Functions
  * @{
  */

/**
  * @}
  */
 
/* Exported functions --------------------------------------------------------*/
/** @defgroup I2S_Exported_Functions I2S Exported Functions
  * @{
  */

/** @defgroup I2S_Exported_Functions_Group1 Initialization and de-initialization functions
 *  @brief    Initialization and Configuration functions
 *
@verbatim     
 ===============================================================================
              ##### Initialization and de-initialization functions #####
 ===============================================================================
    [..]  This subsection provides a set of functions allowing to initialize and
          de-initialize the I2Sx peripheral in simplex mode:

      (+) User must Implement HAL_I2S_MspInit() function in which he configures
          all related peripherals resources (CLOCK, GPIO, DMA, IT and NVIC ).

      (+) Call the function HAL_I2S_Init() to configure the selected device with
          the selected configuration:
        (++) Mode
        (++) Standard
        (++) Data Format
        (++) MCLK Output
        (++) Audio frequency
        (++) Polarity

      (+) Call the function HAL_I2S_DeInit() to restore the default configuration
          of the selected I2Sx peripheral.
@endverbatim
  * @{
  */

/**
  * @brief Receive an amount of data in non-blocking mode with DMA
  * @param  hi2s: pointer to a I2S_HandleTypeDef structure that contains
  *         the configuration information for I2S module
  * @param pData: a 16-bit pointer to the Receive data buffer.
  * @param Size: number of data sample to be sent:
  * @note When a 16-bit data frame or a 16-bit data frame extended is selected during the I2S
  *       configuration phase, the Size parameter means the number of 16-bit data length
  *       in the transaction and when a 24-bit data frame or a 32-bit data frame is selected
  *       the Size parameter means the number of 16-bit data length.
  * @note The I2S is kept enabled at the end of transaction to avoid the clock de-synchronization
  *       between Master and Slave(example: audio streaming).
  * @retval HAL status
  */
HAL_StatusTypeDef HAL_I2S_Receive_DMA(I2S_HandleTypeDef *hi2s, uint16_t *pData, uint16_t Size)
{
  uint32_t *tmp;
  uint32_t tmp1 = 0U;  
 
  if((pData == NULL) || (Size == 0U))
  {
    return  HAL_ERROR;
  }

  if(hi2s->State == HAL_I2S_STATE_READY)
  {
    hi2s->pRxBuffPtr = pData;
    tmp1 = hi2s->Instance->I2SCFGR & (SPI_I2SCFGR_DATLEN | SPI_I2SCFGR_CHLEN);
    if((tmp1 == I2S_DATAFORMAT_24B) || (tmp1 == I2S_DATAFORMAT_32B))
    {
      hi2s->RxXferSize = Size*2U;
      hi2s->RxXferCount = Size*2U;
    }
    else
    {
      hi2s->RxXferSize = Size;
      hi2s->RxXferCount = Size;
    }
    /* Process Locked */
    __HAL_LOCK(hi2s);
    
    hi2s->State = HAL_I2S_STATE_BUSY_RX;
    hi2s->ErrorCode = HAL_I2S_ERROR_NONE;
    
    /* Set the I2S Rx DMA Half transfer complete callback */
    hi2s->hdmarx->XferHalfCpltCallback = I2S_DMARxHalfCplt;
    
    /* Set the I2S Rx DMA transfer complete callback */
    hi2s->hdmarx->XferCpltCallback = I2S_DMARxCplt;
    
    /* Set the DMA error callback */
    hi2s->hdmarx->XferErrorCallback = I2S_DMAError;
    
    /* Check if Master Receiver mode is selected */
    if((hi2s->Instance->I2SCFGR & SPI_I2SCFGR_I2SCFG) == I2S_MODE_MASTER_RX)
    {
      /* Clear the Overrun Flag by a read operation to the SPI_DR register followed by a read
      access to the SPI_SR register. */
      __HAL_I2S_CLEAR_OVRFLAG(hi2s);
    }
    
    /* Enable the Rx DMA Stream */
    tmp = (uint32_t*)&pData;
    printf("Before DMA Start\r\n");

    HAL_DMA_Start_IT(hi2s->hdmarx, (uint32_t)&hi2s->Instance->DR, *(uint32_t*)tmp, hi2s->RxXferSize);

    /* Check if the I2S is already enabled */
    if((hi2s->Instance->I2SCFGR &SPI_I2SCFGR_I2SE) != SPI_I2SCFGR_I2SE)
    {
      /* Enable I2S peripheral */
      __HAL_I2S_ENABLE(hi2s);
    }

     /* Check if the I2S Rx request is already enabled */
    if((hi2s->Instance->CR2 &SPI_CR2_RXDMAEN) != SPI_CR2_RXDMAEN)
    {
      /* Enable Rx DMA Request */  
      hi2s->Instance->CR2 |= SPI_CR2_RXDMAEN;
    }

    /* Process Unlocked */
    __HAL_UNLOCK(hi2s);

    return HAL_OK;
  }
  else
  {
    return HAL_BUSY;
  }
}


/*
 * test_fatfs.c
 *
 *  Created on: 06-Oct-2016
 *      Author: hmicro
 */
#include "fatfs.h"
#include "stm32f4xx_hal.h"
#include "stm32f4xx_hal_def.h"
#include "stm32f4xx_hal_dma.h"
//#include "main.c"

#include "wav_h.h"

extern I2S_HandleTypeDef hi2s2;

    uint16_t RxBuffer1[4096];
    uint16_t RxBuffer2[4096];
    FIL MyFile;

    uint8_t Header_length = 44;
    uint8_t HeaderBuff[44];

void Wave_header()
{
    /* Write chunkID, must be 'RIFF'  ------------------------------------------*/
      HeaderBuff[0] = 'R';
      HeaderBuff[1] = 'I';
      HeaderBuff[2] = 'F';
      HeaderBuff[3] = 'F';
      HeaderBuff[4] = 0x18;
      HeaderBuff[5] = 0x3C;
      HeaderBuff[6] = 0x07;
      HeaderBuff[7] = 0x00;
      /* Write the file format, must be 'WAVE' -----------------------------------*/
      HeaderBuff[8]  = 'W';
      HeaderBuff[9]  = 'A';
      HeaderBuff[10] = 'V';
      HeaderBuff[11] = 'E';
      /* Write the format chunk, must be'fmt ' -----------------------------------*/
      HeaderBuff[12]  = 'f';
      HeaderBuff[13]  = 'm';
      HeaderBuff[14]  = 't';
      HeaderBuff[15]  = ' ';
      /* Write the length of the 'fmt' data, must be 0x10 ------------------------*/
      HeaderBuff[16]  = 0x10;
      HeaderBuff[17]  = 0x00;
      HeaderBuff[18]  = 0x00;
      HeaderBuff[19]  = 0x00;
      /* Write the audio format, must be 0x01 (PCM) ------------------------------*/
      HeaderBuff[20]  = 0x01;
      HeaderBuff[21]  = 0x00;
      /* Write the number of channels, ie. 0x02 (Stereo) ---------------------------*/
      HeaderBuff[22]  = 0x02;
      HeaderBuff[23]  = 0x00;

      /* Write the Sample Rate in Hz ---------------------------------------------*/
      /* Write Little Endian ie. 8000 = 0x00001F40 => byte[24]=0x40, byte[27]=0x00*/
      HeaderBuff[24]  = 0x40;
      HeaderBuff[25]  = 0x1F;
      HeaderBuff[26]  = 0x00;
      HeaderBuff[27]  = 0x00;

      /* Write the Byte Rate -----------------------------------------------------*/
      HeaderBuff[28]  = 0x00;
      HeaderBuff[29]  = 0x7D;
      HeaderBuff[30]  = 0x00;
      HeaderBuff[31]  = 0x00;

      /* Write the block alignment -----------------------------------------------*/
      HeaderBuff[32]  = 0x04;
      HeaderBuff[33]  = 0x00;

      /* Write the number of bits per sample -------------------------------------*/
      HeaderBuff[34]  = 0x10;
      HeaderBuff[35]  = 0x00;

      /* Write the Data chunk, must be 'data' ------------------------------------*/
      HeaderBuff[36]  = 'd';
      HeaderBuff[37]  = 'a';
      HeaderBuff[38]  = 't';
      HeaderBuff[39]  = 'a';

      /* Write the number of sample data -----------------------------------------*/
      /* This variable will be written back at the end of the recording operation */
      HeaderBuff[40]  = 0xD8;
      HeaderBuff[41]  = 0x3B;
      HeaderBuff[42]  = 0x07;
      HeaderBuff[43]  = 0x00;
      /* Return 0 if all operations are OK */
}

void write_data(uint32_t *src_addr, uint32_t size,uint32_t strt_cnt)
{
    uint32_t i,result;
    for(i=strt_cnt;i<size;i++)
    {
//        printf("%c \r\n",RxBuffer1[i]);
        result = f_printf(&MyFile,"%c", &src_addr);
    }
}

void HAL_I2S_RxCpltCallback(I2S_HandleTypeDef *hi2s2)
{
    printf("In the HAL_I2S_RxCpltCallback\r\n");
}

int test_fatfs(void)
{

    uint8_t wtext[] = "This is STM32 working with FatFs"; /* File write buffer */
//    uint8_t wtext1[] = {'2','2','2','2'}; /* File write buffer */


//    uint16_t wtext[50];
    uint16_t x,i,dma_size,*src_addr1,*src_addr2,result, dma_cnt;
    uint16_t rtext[100];
    FRESULT res;
    uint32_t byteswritten=1,bytesread=0;
    char rbuff[30];
    Wave_header();
    res=0;
    dma_size = 1024;
    src_addr1 = RxBuffer1;
    src_addr2 = RxBuffer2;


    /*##-Create and Open a new text file object with write access #####*/
    if(f_open(&MyFile, "STM32.txt", FA_CREATE_ALWAYS | FA_WRITE |FA_OPEN_ALWAYS) != FR_OK)
    {
        /* 'STM32.TXT' file Open for write Error */
        printf("Error opening file \r\n");
        return (-1);
    }
    else
    {
        printf("file now open \r\n");

        for(i=0;i<44;i++)
        {
            wtext[i] = HeaderBuff[i];
            printf("%c \n\r",wtext[i]);
            f_printf(&MyFile,"%c",wtext[i]);
        }

        printf("header added \r\n");

        x =0;
        printf("start i2s capture\r\n");
            res = HAL_I2S_Receive_DMA( &hi2s2, &RxBuffer1, dma_size);
            printf("Result is %d",res);
            printf("DMA, IT, etc init done\r\n");
            while(1)
            {
                HAL_DMA_IRQHandler(&hi2s2.hdmarx);
            }

        for(i=0;i<dma_size;i++)
        {
            printf("%d \n\r",RxBuffer1[i]);
            result = f_printf(&MyFile,"%d", RxBuffer1[i]);
        }

        f_close(&MyFile);

    }



    while(1);

    return (0);
}

/**
  ******************************************************************************
  * File Name          : main.c
  * Description        : Main program body
  ******************************************************************************
  *
  * COPYRIGHT(c) 2016 STMicroelectronics
  *
  * Redistribution and use in source and binary forms, with or without modification,
  * are permitted provided that the following conditions are met:
  *   1. Redistributions of source code must retain the above copyright notice,
  *      this list of conditions and the following disclaimer.
  *   2. Redistributions in binary form must reproduce the above copyright notice,
  *      this list of conditions and the following disclaimer in the documentation
  *      and/or other materials provided with the distribution.
  *   3. Neither the name of STMicroelectronics nor the names of its contributors
  *      may be used to endorse or promote products derived from this software
  *      without specific prior written permission.
  *
  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
  * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE
  * DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE
  * FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL
  * DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR
  * SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER
  * CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
  * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
  *
  ******************************************************************************
  */
/* Includes ------------------------------------------------------------------*/
#include "stm32f4xx_hal.h"
#include "cmsis_os.h"
#include "fatfs.h"
#include "lwip.h"
#include "usb_device.h"

/* USER CODE BEGIN Includes */

#include "power_led_control.h"
#include "io_expander.h"
#include "stmreach_If.h"
#include "spi_ipc.h"


/* USER CODE END Includes */

#define TEST_FATFS
/* Private variables ---------------------------------------------------------*/
CRC_HandleTypeDef hcrc;

I2C_HandleTypeDef hi2c3;

I2S_HandleTypeDef hi2s2;

QSPI_HandleTypeDef hqspi;

RNG_HandleTypeDef hrng;

RTC_HandleTypeDef hrtc;

SD_HandleTypeDef hsd;
HAL_SD_CardInfoTypedef SDCardInfo;

SPI_HandleTypeDef hspi4;
SPI_HandleTypeDef hspi5;
DMA_HandleTypeDef hdma_spi5_rx;
//DMA_HandleTypeDef hdmarx;

TIM_HandleTypeDef htim3;
TIM_HandleTypeDef htim6;
TIM_HandleTypeDef htim7;

UART_HandleTypeDef huart8;
UART_HandleTypeDef huart1;

SRAM_HandleTypeDef hsram1;

osThreadId defaultTaskHandle;

/* USER CODE BEGIN PV */
/* Global function or Task prototype declaration------------------------------*/
extern void userInterfaceTask(void const * argument);
extern void spiIPCRxnTask(void const * argument);
extern void STMEventRxnTask(void const * argument);
extern void STMPacketRxnTask(void const * argument);
extern void configureStmToReach1DSyncPin(void);
extern void configureReach1DToStmSyncPin(void);
extern int test_fatfs(void);
void Wave_header();

/* Private variables ---------------------------------------------------------*/
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
//void Error_Handler(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_TIM3_Init(void);
static void MX_UART8_Init(void);
static void MX_FMC_Init(void);
static void MX_I2C3_Init(void);
static void DMA_Init(void);
static void MX_I2S2_Init(void);
static void MX_QUADSPI_Init(void);
static void MX_SDIO_SD_Init(void);
static void MX_SPI4_Init(void);
static void MX_SPI5_Init(void);
static void MX_TIM6_Init(void);
static void MX_TIM7_Init(void);
static void MX_USART1_UART_Init(void);
static void MX_CRC_Init(void);
static void MX_RNG_Init(void);
static void MX_RTC_Init(void);
void StartDefaultTask(void const * argument);

void HAL_TIM_MspPostInit(TIM_HandleTypeDef *htim);
                

/* USER CODE BEGIN PFP */
/* Private function prototypes -----------------------------------------------*/
osThreadId userInterfaceTaskHandle = NULL;
osThreadId spiIPCRxnTaskHandle = NULL;
osThreadId STMEventRxnTaskHandle = NULL;
osThreadId STMPacketRxnTaskHandle = NULL;

QueueHandle_t g_packetrxQueue = NULL;
QueueHandle_t g_eventrxQueue = NULL;
/* USER CODE END PFP */

/* USER CODE BEGIN 0 */

/*Debug Uart function mapping*/
#ifdef __GNUC__
  /* With GCC/RAISONANCE, small printf (option LD Linker->Libraries->Small printf
     set to 'Yes') calls __io_putchar() */
  #define PUTCHAR_PROTOTYPE int __io_putchar(int ch)
#else
  #define PUTCHAR_PROTOTYPE int fputc(int ch, FILE *f)
#endif /* __GNUC__ */
/* USER CODE END 0 */




int main(void)
{


  /* USER CODE BEGIN 1 */

  /* USER CODE END 1 */

  /* MCU Configuration----------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* Configure the system clock */
  SystemClock_Config();

  /* Reach1D-STM IPC initialization------------------------------------------*/
  stmreach_interfaceInit();

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_DMA_Init();
  MX_FMC_Init();
  MX_I2C3_Init();
  MX_I2S2_Init();
  MX_SDIO_SD_Init();
  MX_SPI4_Init();
  MX_SPI5_Init();
  MX_TIM7_Init();
  MX_USART1_UART_Init();
  DMA_Init();
  /* USER CODE BEGIN 2 */

  /*Configures GPIO pin for synchronizing STM->R1D interface*/
  configureStmToReach1DSyncPin();

  /*Configures GPIO pin for synchronizing R1D->STM interface*/
  configureReach1DToStmSyncPin();

  /*Configure IO expander*/
  Configure_i2c_IO_Expander();

  /*eMMC Init calling out of Driver*/
  BSP_SD_Init();
  /* USER CODE END 2 */

  /* USER CODE BEGIN RTOS_MUTEX */
  /* add mutexes, ... */
  /* USER CODE END RTOS_MUTEX */

  /* USER CODE BEGIN RTOS_SEMAPHORES */
  /* add semaphores, ... */
  /* USER CODE END RTOS_SEMAPHORES */

  /* USER CODE BEGIN RTOS_TIMERS */
  /* start timers, add new ones, ... */
  /* USER CODE END RTOS_TIMERS */

  /* Create the thread(s) */
  /* definition and creation of defaultTask */
  uint16_t wtext[] = { " this is testing"};
  uint16_t buffer[];

  for(int i =0;i<sizeof(wtext);i++)
  {
      buffer[i] = wtext[i];
      printf("%s \r\n",buffer[i]);
  }


  osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 128+1024);
  defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL);



  /* Start scheduler */
  osKernelStart();
 
  /* We should never get here as control is now taken by the scheduler */

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
  /* USER CODE END WHILE */

  /* USER CODE BEGIN 3 */

  }
  /* USER CODE END 3 */

}

/** System Clock Configuration
*/
void SystemClock_Config(void)
{

  RCC_OscInitTypeDef RCC_OscInitStruct;
  RCC_ClkInitTypeDef RCC_ClkInitStruct;
  RCC_PeriphCLKInitTypeDef PeriphClkInitStruct;

  __HAL_RCC_PWR_CLK_ENABLE();

  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSI|RCC_OSCILLATORTYPE_HSE;
  RCC_OscInitStruct.HSEState = RCC_HSE_ON;
  RCC_OscInitStruct.LSIState = RCC_LSI_ON;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
  RCC_OscInitStruct.PLL.PLLM = 25;
  RCC_OscInitStruct.PLL.PLLN = 336;
  RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
  RCC_OscInitStruct.PLL.PLLQ = 7;
  RCC_OscInitStruct.PLL.PLLR = 2;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
  {
    Error_Handler();
  }

  PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_I2S|RCC_PERIPHCLK_RTC
                              |RCC_PERIPHCLK_SDIO|RCC_PERIPHCLK_CLK48;
  PeriphClkInitStruct.PLLI2S.PLLI2SN = 100;
  PeriphClkInitStruct.PLLI2S.PLLI2SR = 2;
  PeriphClkInitStruct.RTCClockSelection = RCC_RTCCLKSOURCE_LSI;
  PeriphClkInitStruct.Clk48ClockSelection = RCC_CLK48CLKSOURCE_PLLQ;
  PeriphClkInitStruct.SdioClockSelection = RCC_SDIOCLKSOURCE_CLK48;
  if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

  HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);

  HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);

  /* SysTick_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(SysTick_IRQn, 15, 0);
}

/* CRC init function */
static void MX_CRC_Init(void)
{

  hcrc.Instance = CRC;
  if (HAL_CRC_Init(&hcrc) != HAL_OK)
  {
    Error_Handler();
  }

}


/* I2S2 init function */
static void MX_I2S2_Init(void)
{

  hi2s2.Instance = SPI2;
  hi2s2.Init.Mode = I2S_MODE_MASTER_RX;
  hi2s2.Init.Standard = I2S_STANDARD_PHILIPS;
  hi2s2.Init.DataFormat = I2S_DATAFORMAT_24B;
  hi2s2.Init.MCLKOutput = I2S_MCLKOUTPUT_DISABLE;
  hi2s2.Init.AudioFreq = I2S_AUDIOFREQ_8K;
  hi2s2.Init.CPOL = I2S_CPOL_LOW;
  hi2s2.Init.ClockSource = I2S_CLOCK_PLL;
  hi2s2.Init.FullDuplexMode = I2S_FULLDUPLEXMODE_ENABLE;
  if (HAL_I2S_Init(&hi2s2) != HAL_OK)
  {
    Error_Handler();
  }

}
static void DMA_Init(void)
{
    DMA_HandleTypeDef hdma_spi5_rx;

    hdma_spi5_rx.Init.Channel = DMA_CHANNEL_2;
    hdma_spi5_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
    hdma_spi5_rx.Init.PeriphInc = DMA_PINC_DISABLE;
    hdma_spi5_rx.Init.MemInc = DMA_MINC_ENABLE;
    hdma_spi5_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
    hdma_spi5_rx.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
    hdma_spi5_rx.Init.Mode = DMA_PFCTRL; //DMA_CIRCULAR;
    hdma_spi5_rx.Init.Priority = DMA_PRIORITY_HIGH;// if needed
    hdma_spi5_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
    if(HAL_I2S_Init(&hdma_spi5_rx)!= HAL_OK)
    {
        Error_Handler();
    }
    if(HAL_DMA_Init(&hdma_spi5_rx)!=HAL_OK)
    {
        Error_Handler();
    }

}

/**
  * Enable DMA controller clock
  */
static void MX_DMA_Init(void)
{
  /* DMA controller clock enable */
  __HAL_RCC_DMA1_CLK_ENABLE();

  /* DMA interrupt init */
  /* DMA2_Stream3_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(DMA1_Stream4_IRQn, 5, 0);
  HAL_NVIC_EnableIRQ(DMA1_Stream4_IRQn);

}

/** Configure pins as
        * Analog
        * Input
        * Output
        * EVENT_OUT
        * EXTI
     PD7   ------> FMC_NE1
     PD0   ------> FMC_D2_DA2
     PD1   ------> FMC_D3_DA3
     PF0   ------> FMC_A0
     PD4   ------> FMC_NOE
     PF1   ------> FMC_A1
     PF2   ------> FMC_A2
     PD15   ------> FMC_D1_DA1
     PD14   ------> FMC_D0_DA0
     PE8   ------> FMC_D5_DA5
     PE9   ------> FMC_D6_DA6
     PE7   ------> FMC_D4_DA4
     PE10   ------> FMC_D7_DA7
*/


void HAL_Delay(__IO uint32_t Delay){
    while(Delay)
    {
        if( SysTick->CTRL & SysTick_CTRL_COUNTFLAG_Msk)
        {
            Delay--;
        }
    }
}

/* USER CODE END 4 */



/* StartDefaultTask function */
void StartDefaultTask(void const * argument)
{
    /* init code for FATFS */
    MX_FATFS_Init();
//#if TEST_FATFS
    test_fatfs();
//#endif
    /* init code for USB_DEVICE */
    MX_USB_DEVICE_Init();
    while (1)
    {
        for(;;)
        {
            osDelay(5000);
        }
    }

/* USER CODE BEGIN 5 */
/* USER CODE END 5 */
}

/**
  * @brief  This function is executed in case of error occurrence.
  * @param  None
  * @retval None
  */
void ERROR_HANDLER(char * func, int line)
{
  /* USER CODE BEGIN Error_Handler */
  /* User can add his own implementation to report the HAL error return state */
  printf("Error Handler %s: %d\r\n", func, line);
  while(1)
  {
        osDelay(2000);
  }
  /* USER CODE END Error_Handler */
}

#ifdef USE_FULL_ASSERT

/**
   * @brief Reports the name of the source file and the source line number
   * where the assert_param error has occurred.
   * @param file: pointer to the source file name
   * @param line: assert_param error line source number
   * @retval None
   */
void assert_failed(uint8_t* file, uint32_t line)
{
  /* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
    ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  /* USER CODE END 6 */

}

#endif

/**
  * @}
  */

/**
  * @}
*/

/*****************************END OF FILE****/

Outcomes