AnsweredAssumed Answered

TIM4 in Encoder Mode - Nucleo F767ZI

Question asked by Neo M on Oct 6, 2016
Latest reply on Oct 7, 2016 by FTITI.Walid
I am trying to set up TIM4 in Encoder Mode in Nucleo F767ZI. I used STM32CubeMX to set up the Timer. The TIM->CNT value oscillates between two values. On checking further, I found the DIR bit to be oscillating between 0 and 1. If I read the values of both the channels and do an external counting, it works fine. I am reading both edges on both the channels. 

Outcomes