AnsweredAssumed Answered

Nucleo STML031K6: Cannot find pin PA13(SYS_SWDIO) and PA14(SYS_SWCLK)

Question asked by le.bien on Aug 25, 2016
Latest reply on Aug 25, 2016 by FTITI.Walid
Hi
I'm using Nucleo STM32L031K6 for my project and I want to use an external debugger for the board instead of the internal debugger provided on the board.

I looked at the data sheet of this STML031 and it says that the pins SWDIO and SWCLK are corresponding to the pins PA13 and PA14 on the board respectively. However I could not find where are these two pins on the STML031K6 board?
Also The MCU package is 32-pins, but there are only 30 pins on the board.

Where are these two PA13(SWDIO) and PA14(SWCLK) pins?
Thanks,
Bien

Outcomes