AnsweredAssumed Answered

Can't make the ADC run on stm32f4-discovery

Question asked by georgiev.zdravko on Apr 28, 2016
Latest reply on Apr 30, 2016 by baird.hal.001
I have a stm32f4-discovery with the stm32f407vg uC on it and I'm trying to program the ADC1 and measure some signals on the port PC7 with it. According to the documentation PC7 hangs on the ADC12_IN15 which I'm interpreting as ADC1 and ADC2 channel 15. I want to use the ADC_DMA example projects from the STD library STM32F4xx_DSP_StdPeriph_Lib_V1.6.1. The signal to the PC7 is provided by a signal generator and it's a square signal with frequency of 5 Hz, Vpp of 3 V and offset of 1.5 V. Then I'm running the following code, which is successfully compiled and uploaded:


#define ADCx                     ADC1
#define ADC_CHANNEL              ADC_Channel_15
#define ADCx_CLK                 RCC_APB2Periph_ADC1
#define ADCx_CHANNEL_GPIO_CLK    RCC_AHB1Periph_GPIOC
#define GPIO_PIN                 GPIO_Pin_5
#define GPIO_PORT                GPIOC
#define DMA_CHANNELx             DMA_Channel_1
#define DMA_STREAMx              DMA1_Stream0
#define ADCx_DR_ADDRESS          ((uint32_t)0x4001224C)

static void ADC_Config(void);




/**
  * @brief  Main program
  * @param  None
  * @retval None
  */
int main(void)
{
  /*!< At this stage the microcontroller clock setting is already configured, 
       this is done through SystemInit() function which is called from startup
       files (startup_stm32f40_41xxx.s/startup_stm32f427_437xx.s/startup_stm32f429_439xx.s)
       before to branch to application main. 
       To reconfigure the default setting of SystemInit() function, refer to
       system_stm32f4xx.c file
     */






  /* ADC configuration */
  ADC_Config();


  /* Start ADC Software Conversion */ 
  ADC_SoftwareStartConv(ADCx);


  while (1)
  {
    uwADCxConvertedVoltage = uhADCxConvertedValue *3300/0xFFF;
  }
}


/**
  * @brief  ADC3 channel07 with DMA configuration
  * @note   This function Configure the ADC peripheral  
            1) Enable peripheral clocks
            2) DMA2_Stream0 channel2 configuration
            3) Configure ADC Channel7 pin as analog input
            4) Configure ADC3 Channel7 
  * @param  None
  * @retval None
  */
static void ADC_Config(void)
{
  ADC_InitTypeDef       ADC_InitStructure;
  ADC_CommonInitTypeDef ADC_CommonInitStructure;
  DMA_InitTypeDef       DMA_InitStructure;
  GPIO_InitTypeDef      GPIO_InitStructure;


  /* Enable ADCx, DMA and GPIO clocks ****************************************/ 
  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA1, ENABLE);
  RCC_AHB1PeriphClockCmd(ADCx_CHANNEL_GPIO_CLK, ENABLE);  
  RCC_APB2PeriphClockCmd(ADCx_CLK, ENABLE);
  


  /* DMA1 Stream0 channel1 configuration **************************************/
  DMA_InitStructure.DMA_Channel = DMA_CHANNELx;  
  DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)ADCx_DR_ADDRESS;
  DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&uhADCxConvertedValue;
  DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;
  DMA_InitStructure.DMA_BufferSize = 1;
  DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
  DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Disable;
  DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
  DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
  DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
  DMA_InitStructure.DMA_Priority = DMA_Priority_High;
  DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;         
  DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;
  DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
  DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
  DMA_Init(DMA_STREAMx, &DMA_InitStructure);
  DMA_Cmd(DMA_STREAMx, ENABLE);


  /* Configure ADC1 Channel15 pin as analog input ******************************/
  GPIO_InitStructure.GPIO_Pin = GPIO_PIN;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
  GPIO_Init(GPIO_PORT, &GPIO_InitStructure);


  /* ADC Common Init **********************************************************/
  ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;
  ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;
  ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;
  ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;
  ADC_CommonInit(&ADC_CommonInitStructure);


  /* ADC1 Init ****************************************************************/
  ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
  ADC_InitStructure.ADC_ScanConvMode = DISABLE;
  ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
  ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
  ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1;
  ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
  ADC_InitStructure.ADC_NbrOfConversion = 1;
  ADC_Init(ADCx, &ADC_InitStructure);


  /* ADC1 regular channel15 configuration **************************************/
  ADC_RegularChannelConfig(ADCx, ADC_CHANNEL, 1, ADC_SampleTime_3Cycles);


 /* Enable DMA request after last transfer (Single-ADC mode) */
  ADC_DMARequestAfterLastTransferCmd(ADCx, ENABLE);


  /* Enable ADC1 DMA */
  ADC_DMACmd(ADCx, ENABLE);


  /* Enable ADC1 */
  ADC_Cmd(ADCx, ENABLE);
}


And I'm expecting to see some data stored in uwADCxConvertedVoltage, or some movement in the ADC1 or the DMA1, but unfortunately there is nothing... :(.

What could be wrong? 

Outcomes