AnsweredAssumed Answered

Unable to link emWin - missing LCD_IO_WriteReg

Question asked by macfarlane.ken on Apr 7, 2016
Latest reply on Apr 14, 2016 by Clive One
I'm trying to build a first graphical LCD project with Visual GDB (which lets you use Visual Studio for embedded development using the ARM GCC toolchain).

I can't find any sign of any of the LCD_IO_ routines in the HAL firmware (I've got the F1 stuff).  Perhaps its missing and Segger's stuff wasn't used for the demo on the 3210C, but from the presence of the STemWin_HelloWorld
in the
F1Cube firmware
in
Projects\STM3210C_EVAL\Applications\STemWin

I have built this with IAR's EWARM, but I don't have the mapfile anymore to see where it got the functions from.

I've got the ili9320 & 9325.c's added into the project, so there must be an SPI layer between these 2 files and the LCD.
Segger defer to ST for first line support of emWin.  

Outcomes