AnsweredAssumed Answered

STM32F429i Disco SPI driver for Display

Question asked by Gluka_73 on Apr 3, 2016
Latest reply on Apr 4, 2016 by ForumSTM32.ForumSTM3
Hello everybody,
I would like to "free" some peripherals in the SMT32F429i-DISCO and drive the ili9341 display in SPI mode instead of LTDC.
I'm working with CubeMX to init the SPI5 and DMA for the SPI transfer.
After it I've developed the display init starting from a lib example in Keil but without using CubeMX.
I would like to port that lib in Cube + True Studio but, by now, it doesn't work.
Have someone do the same job and can help me?

Thanks.
Luca

Outcomes