AnsweredAssumed Answered

STM32F407G-DISC1 requires PC connection to boot

Question asked by trent on Mar 28, 2016
Latest reply on Nov 10, 2017 by Clive One
Recently the STM32F407 discovery board changed part numbers from STM32F4DISCOVERY to STM32F407G-DISC1. The old boards could be powered directly via the 5V pins on the headers, or via a USB wall-wart, but the new boards need to be connected to a PC in order to boot. Is this intended behavior? Is there a solution aside from flashing an older firmware to the STLink chip?
Thanks

Outcomes