AnsweredAssumed Answered

STM32F469 Discovery Kit with IAR EW Writing Outside Flash memory

Question asked by mandrekar.aditya on Mar 3, 2016
Latest reply on Mar 4, 2016 by mandrekar.aditya
Hi,

I'm trying to program an STM32F469NI Discovery board with a default project from the Cube set of projects using IAR Embedded Workbench (v 7.50). The project builds fine, but while trying to program the device I get an error that says "Writing outside flash memory at address 0x90000000".

I can "program" the device if I don't use the flash loader, but then any changes I make are not reflected on the device, i.e. I started with just trying to replace text that is visible on the screen with debug words to see if my changes were having effect, they're not.

I tried to play around with the ICF file and other settings in the "Project Options" menu but to no avail.

I would appreciate any assistance towards this issue.

Outcomes