AnsweredAssumed Answered

PM6670AS current consumption

Question asked by Walsh.Eamonn on Oct 2, 2013
Hi,
I am thinking of using a PM6670AS to power DDR3 memory on a new Virtex-7 board. Can someone tell me what will be the maximum current consumed on the VCC and AVCC +5V pins? This must be with the S3 and S5 pins connected to AVCC, a nominal load (<1mA) on Vttref, the Mode pin tied to AVcc and the DDRSEL pin tied to ground (1.5v operation).

Thanks,
Eamonn Walsh

Outcomes