AnsweredAssumed Answered

XCore407I programming

Question asked by woj.woj on Feb 21, 2016
Latest reply on Feb 22, 2016 by woj.woj
Hello all users, this is my first post on this forum.
I'm new to STM microcontrollers and I have bought XCore407I  board. I have got STM32L0 DISCOVERY board with debugg connector CN5, whitch can be use to programm/debugg external applications. I tried to connect DISCOVERY CN5 pins to XCORE board and use Attolic True Studio to programm processor on the xcore board but the software can't connect to the target (Error 4).
As I read in Discovery board manual to programm external application I have to remove 2 jumpers from the board and connect CN5 pins to my application (XCORE board in this case) according to table 3 (on 15 page) in Discovery manual. I made those steps but software do not see processor on XCore board. Has anybody any suggestions?

Outcomes