AnsweredAssumed Answered

SPC5STudio 3.4.0 is available !

Question asked by Erwan Y Employee on Jan 26, 2015
Latest reply on Feb 9, 2015 by Mike
SPC5STudio 3.4.0 is available !
Dear Users,

The 3.4.0 release is now available on the update site.

Here are is the change log
SPC5STUDIO CORE :
- Patch mode: newly created project is already patched
- Implementing invisible groups
- Allow user to patch components/lib/ files: V2
- Patch mode : patch.xml to be hidden / Default / Grey Decorators
- Implement Hidden properties

SPC5STUDIO Repository :
- Create NIL RTOS SPC560Bxx Test Application for Discovery

SPC5STUDIO Pinmap :
- Unable to Set more than 10 pin in PinMap Wizard

SPC5-HAL :
- CAN Naming convention : Change the id number of Filter Settings
- The message buffers Tx/Rx Configuration in CAN module are fixed
- The incorrect registers bits definitions and driver data structures and types in hal_lld.h head file
- eMIOS channels 1,3,5,6,2,4,11,13 are not usable for ICU
- PWM/ICU functions on eMIOS

NIL RTOS :
- New feature for SPC560Bxx

We wish you a happy usage.

The SPC5Studio team.

Outcomes