AnsweredAssumed Answered

Start using SPC

Question asked by Mike on Jan 23, 2015
Latest reply on Jan 30, 2015 by Erwan Y
Hello All,
I am new user for SPC series MCU and SPC5Studio as well. I am trying to start with few example codes to understand the HAL, PAL implementations. I am trying to go through different posts on this forum to understand the way people are accessing the features. But somehow I am find it very very difficult to locate the resources - be it a sample code or a file reference or even a document reference. E.g A post below mentions about document sections,
You can use External INTERRUPT In SIUL chapter 48
and the convenient EIRQ[X] chapter 48.4


you should use vector41 , vector42, vector 43 or vector 44


41 0x0290 16 SIU External IRQ_0 SIUL
42 0x02A0 16 SIU External IRQ_1 SIUL
43 0x02B0 16 SIU External IRQ_2 SIUL
44 0x02C0 16 SIU External IRQ_3 SIUL


2) for mapping you should use IO Settings and set your good port/function in the good mode
    chap 4 from the convenient table "function summary"

I tried referring to the reference manual for SPC560 series (RefManual_CD00259063.pdf) to locate these sections but could not find. Is there any other document/manual that mentions all this information? I tried searching SPC5Studio help as well.
I beg your pardon for asking such simple questions through different posts but if you can provide the details, it will help me move further. Thanks for all your help.
Mike.

Outcomes