AnsweredAssumed Answered

M24LR-DISCOVERY question

Question asked by kilshtein.daniel on May 4, 2015
Latest reply on Jun 30, 2015 by NFC/RFID ST Support

Hi

I need to store a single file on the board from a PC (with ST application via USB) then I need to be able to read the file back to the PC (with ST application via USB). In addition, I need to be able to transfer the same file (via NFC) to any reader (i.e. smart phone)

I have only the "RF transceiver board" that is connected to the PC with USB.

I downloaded the demo application for it (stsw-m24lr011) but I can't make it communicate with the board via USB. Is there a way to store file on this board at all and if so, hot to accomplish this task?

Thanks a lot.

Outcomes