AnsweredAssumed Answered

SETVAL interface to STM32 DISCOVERY

Question asked by caldognetto.nicola on Sep 15, 2012
I apologize right now for my English.

I purchased a STM32VLDISCOVERY and unsteval-mki0 +2 v2 both st microelectronics.
I tried the program that is given with the second component, and seemed very nice.
Wanted hours interfacing the STEVAL-mki062v2 with the STM32VLDISCOVERY so that, for example, if the sensor has a temeprature of more than 30 degrees turns on an LED, if not remains off.
How do I do or where I can find material with explanations?

Thanks for your help

Outcomes