AnsweredAssumed Answered

LPR430AL roll angle wrong

Question asked by everybody_jamming on Aug 7, 2012
I work with the gyroscope LPR430AL. The pitch angle works fine, the roll angle results in some strange values... (if I turn the module of 90° in roll angle I measure the right value of 90°. When I come back to 0° I measure ca. -25° like an offset. I turn again the module to 90° and I measure just 65°, come back to 0° and I measure -50° and so on...)

Any idea?

Thank you!

Outcomes