AnsweredAssumed Answered

Using CAN on SPC560B-DIS

Question asked by rosen.shachar on Nov 19, 2014
Latest reply on Oct 15, 2015 by Erwan Y
Hello,
I am trying to make a simple project that for a start can send a single CAN frame.
I am using the SPC560B-DIS evb without any CAN board (will connect later on my own converter).
I took a CAN sample  from other evb and merged it to my project but it doesn't work!
Is there any CAN sample that works that I can use?
Can I connect a scope to the TX pin and view the data without converter to CAN High and CAN Low?
In the example i did not see any initialization to the I/O (Tx and Rx) is that correct?
Can I use the external clock on my board for the CAN module?

Thanks
Shachar

Outcomes