AnsweredAssumed Answered

LIS2DM I2C and low power

Question asked by gantner.reinhold on Jun 13, 2014
Latest reply on Mar 19, 2015 by mharvey
after power up the LIS2DM the current consumption is about 100uA ?!
The connection is:
Pin1 : SCL with a external 4K7 to 3V
Pin2 : SDA with a external 4K7 to 3V
Pin3 : SA0 connected to GND
Pin4 : /CS connected to 3V
Pin5: INT2 open
Pin6: INT1 to Input Port uP
Pin7,8: 3V
Pin9-14: GND
Could it be that there is an internal pull-up on Pin3 and I should connect the SA0 line to 3V to get a low power consumption ?

Outcomes