AnsweredAssumed Answered

HVLED815PF on Power Supply eDesignSuite

Question asked by Pedro Pereira on Nov 16, 2016
Latest reply on Nov 16, 2016 by Pedro Pereira
Hi There,

It would be great to be able to choose HVLED815PF on eDesignSuite, when selecting:
Power Conversion -> Power Supply -> AC/DC -> Isolated -> QR Flyback (with HPF), instead of only as LED Driver. The purpose is to use it in designs with less than 11W (actual Pout in general/home lighting produtcs) with CV, PSR, Wide Mains and HPF, instead of using the HVLED0001/A models that despite working, were made for much higher power supplies (75W). The HVLED815PF shows this kind of use (CV) on the application note:
"AN4350: High power factor LED driver with constant voltage regulation based on HVLED815PF" (that has some errors on formulas still to solve - we already submitted a request for the correction or an errata) but unfortunately the eDesignSuite doesn't seem to let us use it on the same way.

Best Regards,

Pedro Pereira

Outcomes