AnsweredAssumed Answered

LSM9DS0 debugging

Question asked by hurovitz.sasha on Jul 11, 2016
Hi all,
I've recently bought a couple of LSM9DS0's for a simple project.
Before soldering them to my board I tried to checked if everything was right.
I ONLY connected pin 5 and 6 to GND and 15, 16 and 17 to 3v3.
However when I turned on the power supply, it showed up a short circuit.
I was wondering if anyone has an idea on what is wrong.
I don't think that I burnt them by static as I used them with a wrist band connected to GND.
Besides, the cut-off current on the power supply is set to 200mA.
I'm also attaching the design of the board I was planning to use with the IMU if anyone has an opinion about it.
Best regards

Attachments

Outcomes