AnsweredAssumed Answered

STM32F Nucleo Firmware Upload with TrueSTUDIO

Question asked by farah.ibrahim on Feb 1, 2016
Latest reply on Feb 2, 2016 by sramek.jiri.002
I installed the Atollic TrueSTUDIO IDE for developing software for the STM32F303RE-Nucleo board, and have been trying to run the example file located in: STM32Cube_FW_F3_V1.4.0\Projects\STM32F303RE-Nucleo\Examples\GPIO\GPIO_IOToggle\TrueSTUDIO which I downloaded from the ST site. After opening the project in TrueSTUDIO and building it, I try to run it using the F11 key and I get the following console output:

Atollic TrueSTUDIO gdbserver for ST-Link.  Version 2.2.0 Pro
Copyright 2010-2015, Atollic AB. 




Starting server with the following options: 
        Persistant Mode            : Disabled 
        LogFile Name               : debug_log.txt
        Logging Level              : 1
        Listen Port Number         : 61234
        Status Refresh Delay       : 15s
        Verbose Mode               : Disabled 
        SWD Debug                  : Enabled 


Connecting to the ST-Link Debugger... OK

However, I then get a pop-up saying:

STM32F%20upload%20error.PNG

I've been trying to debug this and I can't figure out what is causing this error, since the board is plugged in to the laptop via USB.

Any help is greatly appreciated.

Outcomes