AnsweredAssumed Answered

Nucleo F091 SPI pins

Question asked by Aliaga.David on Jan 26, 2016
Latest reply on Jan 26, 2016 by Clive One
Hello.
I am looking at the Nucleo F091 pin distribution,
Pin distribution page
 and notice SPI1 and SPI2 pins. No problem about SPI2 pins (in fact I have used them successfully) but for SPI1 I can see that there are two sets of pins for it. 

1) Is this correct?  I mean I see for example SPI1 MOSI is PA_7 and PB_5 .

2) Also I wonder which pin is SPI1 CS?? I am thinking PA_4 but then I read it is PB_6 so I am confused...

Any help will be greatly appreciated

Outcomes