AnsweredAssumed Answered

problems downloading STM32F7 discovery demo into board

Question asked by Osto on Dec 27, 2015
Latest reply on Dec 28, 2015 by Clive One
Hi,

I'm using Keil V5 and loaded the standard demo software (Garden control, home alarm, vnc server, ....). I can compile the project without problem but when downloading int it to board, I get message that there is no algorithm for 0x9000 0000.
When I add the available 4M SPI memory to the system, doesnt work either.
When I load the hex file of the demo (downloaded from ST) and store it with st-link utility, everything is working but when I download the compiled hex file, I get a message that there is no algorithm for that memory.
Whatever I do, either I get the software running with scrambled icons or I cant load it at all.
I need your help, how to go on to download the compiled software with Keil V5 so that I can debug it.

Thanks a lot.
Osto

Outcomes