AnsweredAssumed Answered

stm32f103 usb device issue

Question asked by rajendhiran.thangame on Dec 21, 2015
Latest reply on Dec 28, 2015 by rajendhiran.thangame
Hi Everyone.

I am working in stm32f103xx  .

it has usb 2.0 full speed.

 now i need to  enumerate usb as virutal com port . i downloaded usb example from st.
STM32F10xUSBLib_V2.2.1..
 
Edit.

i changed in platform config according to my evaluation stm32f10b . then in hw_config i edit the usb disconnect pin as pb4. pin pb4 is jtag as default then i remapped as gpio..

GPIO_PinRemapConfig(GPIO_Remap_SWJ_NoJTRST, ENABLE);
     GPIO_PinRemapConfig(GPIO_Remap_SWJ_JTAGDisable, ENABLE);.

then i compiled and load into my board. but nothing happen while connecting into my laptop using windows 7.. 

there is nothing to change in the example. 






 

Outcomes