AnsweredAssumed Answered

[SOLVED] Stm32F429 discovery SPI2 problem with NRF24L01 register read

Question asked by chopra.sanjay on Dec 20, 2015
Latest reply on Dec 20, 2015 by chopra.sanjay
I am trying to read register for NRF24l01 with STM32F429 Discovery. I am using SPI2 with PB13,PB14,PB15 as SPI2_SCK,
SPI2_MISO, SPI2_MOSI and PB12 as CE pin. When i read i get  0 always. Please suggest me what's wrong with this code.



static bool isSet = false;
 
void error()
{
    while(1)
    {
        if(isSet)
            GPIO_ResetBits( GPIOG, GPIO_Pin_14 |GPIO_Pin_13 );
        else
            GPIO_SetBits( GPIOG, GPIO_Pin_14 |GPIO_Pin_13 );
        isSet = !isSet;
        delay( 50 );
    }
}
 
/* Exported macro ------------------------------------------------------------*/
#define CS_LOW()       GPIO_ResetBits(GPIOB, GPIO_Pin_12)
#define CS_HIGH()      GPIO_SetBits(GPIOB, GPIO_Pin_12)
 
uint8_t SendByte(uint8_t byte)
{
    while(!SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_TXE));
    SPI_I2S_SendData(SPI2, byte);
    while(!SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_RXNE));
    return SPI_I2S_ReceiveData(SPI2);
}
 
void InitSPI2()
{
 
    RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE);
    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB , ENABLE);
 
    GPIO_InitTypeDef GPIO_InitTypeDefStruct;
 
    GPIO_InitTypeDefStruct.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15;
    GPIO_InitTypeDefStruct.GPIO_Mode = GPIO_Mode_AF;
    GPIO_InitTypeDefStruct.GPIO_Speed = GPIO_Speed_50MHz;
    GPIO_InitTypeDefStruct.GPIO_OType = GPIO_OType_PP;
    GPIO_InitTypeDefStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;
    GPIO_Init(GPIOB, &GPIO_InitTypeDefStruct);
 
    GPIO_InitTypeDefStruct.GPIO_Pin = GPIO_Pin_12;
    GPIO_InitTypeDefStruct.GPIO_Mode = GPIO_Mode_OUT;
    GPIO_InitTypeDefStruct.GPIO_Speed = GPIO_Speed_50MHz;
    GPIO_InitTypeDefStruct.GPIO_PuPd = GPIO_PuPd_UP;
    GPIO_InitTypeDefStruct.GPIO_OType = GPIO_OType_PP;
    GPIO_Init(GPIOB, &GPIO_InitTypeDefStruct);
 
    GPIO_PinAFConfig(GPIOB, GPIO_PinSource13, GPIO_AF_SPI2);
    GPIO_PinAFConfig(GPIOB, GPIO_PinSource14, GPIO_AF_SPI2);
    GPIO_PinAFConfig(GPIOB, GPIO_PinSource15, GPIO_AF_SPI2);
 
    GPIO_SetBits(GPIOB, GPIO_Pin_12);
 
 
    SPI_InitTypeDef SPI_InitTypeDefStruct;
    SPI_InitTypeDefStruct.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
    SPI_InitTypeDefStruct.SPI_Mode = SPI_Mode_Master;
    SPI_InitTypeDefStruct.SPI_DataSize = SPI_DataSize_8b;
    SPI_InitTypeDefStruct.SPI_CPOL = SPI_CPOL_Low;
    SPI_InitTypeDefStruct.SPI_CPHA = SPI_CPHA_1Edge;
    SPI_InitTypeDefStruct.SPI_NSS = SPI_NSS_Soft;
    SPI_InitTypeDefStruct.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_8;
    SPI_InitTypeDefStruct.SPI_FirstBit = SPI_FirstBit_MSB;
    SPI_InitTypeDefStruct.SPI_CRCPolynomial = 7;
    SPI_CalculateCRC(SPI2, DISABLE);
    SPI_Init(SPI2, &SPI_InitTypeDefStruct);
 
    SPI_Cmd(SPI2, ENABLE);
}
 
int main(void)
{
    // it will start sysTick
    systemInit();
 
    initSerial();
 
    // for error blink
    RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_GPIOG, ENABLE );
    GPIO_InitTypeDef        GPIO_InitStructure;
    GPIO_InitStructure.GPIO_Pin = (GPIO_Pin_14 |GPIO_Pin_13);
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
    GPIO_Init(GPIOG, &GPIO_InitStructure);
 
    InitSPI2();
 
    while( 1 )
    {
        for ( int i =0; i < 5; i++)
        {
            CS_LOW();
            SendByte(i);
            uint8_t d = SendByte(0xFF);
            CS_HIGH();
            tfp_printf("Reg(%d) %d\n", i, d);
            delay(100);
        }
    }
}

Outcomes