AnsweredAssumed Answered

STM32 Nucleo and mbed

Question asked by Aliaga.David on Dec 15, 2015
Latest reply on Dec 15, 2015 by Clive One
Hello everybody. This is my first post. 
I would like to ask about mbed. 
I have one (STM32F091RC) and I have used mbed to program it with a couple of examples (LED switching, button etc). The programs seem quite simple.

However I have also seen programs for the STM32 architecture. They are understandable, but are obviously more complex than the mbed's. They require pin I/O initialization etc. Not that I am complaining just that I noticed. 

Why are the mbed programs so simple?
Can I do serious development with it?
If yes, they why bother with the other more complex programs?
In the event that I want to write a program for production after I finish a prototype will I be able to use mbed too?
Any other comment referring mbed that I should be aware of

Outcomes