AnsweredAssumed Answered

[SOLVED] STM32F746G-Discovery Board is giving HardFault after a few minutes of use

Question asked by nikolaou.christos on Sep 26, 2015
Latest reply on Sep 27, 2015 by nikolaou.christos
Hi,

Recently I got two STM32F746G-Discovery boards.
I run the same firmware on both.
On one the firmware runs ok without any issues.
On the other, I got stops and via the debugger seen that is staying in loop inside HardFault_Handler function.

/**
  * @brief  This function handles Hard Fault exception.
  * @param  None
  * @retval None
  */
void HardFault_Handler(void)
{
  /* Go to infinite loop when Hard Fault exception occurs */
  while (1)
  {
  }
}


What can be done for this? Is there any procedure for faulty boards?

Outcomes