AnsweredAssumed Answered

LSM303DLHC data ready interrupts for STM32F3-Discovery

Question asked by adam.at.epsilon on Jul 27, 2015
Latest reply on Sep 2, 2015 by adam.at.epsilon
LSM303DLHC Data Sheet says

The LSM303DLHC features two data-ready signals (RDY) which indicate when a new set of measured acceleration data and magnetic data are available

but Figure 4 only shows one DRDY pin out, does that mean that when the pin is set, both accelerometer and compass has new data, or do I have to check status/ctrl registers to see if accelerometer or magnetometer has data?

Outcomes