AnsweredAssumed Answered

STM32F0 discovery and ST-link utility

Question asked by grandmougin.jean_fra on Jun 12, 2015
Latest reply on Jun 25, 2015 by Ibn Ziyed
Hello

I'm trying to use the STM32F0 discovery with the ST link on board.
So in first time, I try with ST link utility V3.6.0 with STLinkUSBDriver.dll V4.3.4.0 on windows 7 pro 64 bits.
All seem to be right, STLink utility is connected with the good target (STM32F051...) but when I want to program the target an internal error occured.

07:59:34 : ST-LINK SN : 50FF6D065067525543600187

07:59:34 : ST-LINK Firmware version : V2J23S0

07:59:34 : Connected via SWD.

07:59:34 : SWD Frequency = 1,8 MHz.

07:59:34 : Connection mode : Normal.

07:59:34 : Device ID:0x440

07:59:34 : Device flash Size : 64KBytes

07:59:34 : Device family :STM32F051x4/F051x6/F051x8/F030x8

08:13:22 : [test_stm32.hex] opened successfully.

Address Ranges [0x00000000 0x00000F05] [0x00000F08 0x00000F80]

08:13:28 : No OnChip verification function found. Verify after programming will be performed.

08:13:28 : Internal command error

08:13:28 : Error occured during program operation!

08:13:28 : Programming error @: 0x00000000

I try with Eclipse and with IAR the problem is the same with 2 differents boards

Can someone help me ?

Thanks

Outcomes