AnsweredAssumed Answered

STM32F10B Eval Programming Issue

Question asked by sayanwar.shashank on May 31, 2015
Latest reply on Jun 2, 2015 by Clive One
Hi,

I am using STM32f10B with STM32f103VGT6 on it. The problem is that the MCU is not working as per the program. It has a fixed GPIO high and they stay in the same state. I tried using coocox and IAR workbench. They do not show any error in the flashing of the code. Even if I erase the memory, I still have the GPIO in the high state. Also, the STM32 util says the memory has been erased. Still, the condition of the GPIO is high.

Please help.

Outcomes