AnsweredAssumed Answered

USART application DELAY error on STM32F4

Question asked by chung.karen on May 6, 2015
Latest reply on May 7, 2015 by Clive Two.Zero
I have develop an app and one button is sending the string A. However when i connect the STM32F407 and run the program it only can execute one command line instead of all command under the char A. Is there anyway to tackle this problem? I KNOW IT IS RELATED TO DELAY PROBLEM. BUT HOW CAN I SOLVE IT BY PROGRAMMING? THANKS!!!


#include "stm32f4xx.h"
#include "usart_config.h"
#include "String.h"
#include "config.h"
#include "delay.h"


void usart_lowLevelInit(){
  GPIO_InitTypeDef GPIO_InitStructure;
 
  /**************************GPIO Configuration*****************************/
   RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
   RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);
   
  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
  GPIO_Init(GPIOC, &GPIO_InitStructure);
 
  /* Connect USART pins to AF */
  GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_USART3);
  GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_USART3);
  //*************************USARTx configuration *****************************
  USART_InitTypeDef USART_InitStructure;
 
  /* USARTx configuration -------------------------------/
  / * USARTx configured as follow:
        - BaudRate = 9600 baud
        - Word Length = 8 Bits
        - Two Stop Bit
        - Odd parity
        - Hardware flow control disabled (RTS and CTS signals)
        - Receive and transmit enabled
  */
  USART_InitStructure.USART_BaudRate = 9600;
  USART_InitStructure.USART_WordLength = USART_WordLength_8b;
  USART_InitStructure.USART_StopBits = USART_StopBits_1;
  USART_InitStructure.USART_Parity = USART_Parity_No;
  USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
 
  USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
 
  USART_Init(USART3, &USART_InitStructure);
 
  USART_Cmd(USART3, ENABLE);


 /*USART_ITConfig(USART3, USART_IT_TC, ENABLE);*/
  USART_ITConfig(USART3, USART_IT_RXNE, ENABLE);
  //***************************Interruption Config***********************************
  NVIC_InitTypeDef NVIC_InitStructure;
 
  /* Configure the NVIC Preemption Priority Bits */
  
  //NVIC_PriorityGroupConfig(NVIC_PriorityGroup_0);
 
  /* Enable the USART3 Interrupt */
  NVIC_InitStructure.NVIC_IRQChannel = USART3_IRQn;
  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
  NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
  NVIC_Init(&NVIC_InitStructure);
 }
//------------------Fonction de Reception ---------------------------------
extern __IO uint8_t cursor,flag;
extern __IO char buffer[20],result[20];
extern __IO char c;





void usart_receive(char c)
{
  
  if (c=='A')
  {
    


 
 
 moteur2(1550);
  delay_nms(100);
  moteur17(1500);
  delay_nms(100) ;
 moteur3(2150);
 delay_nms(100) ;
 moteur18(1300);
  delay_nms(100) ;
  moteur2(1750);
    delay_nms(100);
  moteur17(1200);
  
  
 delay_nms(100) ;
  moteur8(1200);
  delay_nms(100);
  moteur11(1600);
   delay_nms(100) ;
 moteur12(500);
 delay_nms(100) ;
 moteur9(1400);
 delay_nms(100);
  moteur8(1500);
    delay_nms(100);
   moteur11(1300);
   
 
 delay_nms(100) ;
  moteur5(1500);
delay_nms(100);
  moteur14(2100);
  delay_nms(100);
 moteur15(1000);
 delay_nms(100) ;
 moteur6(1100);
 delay_nms(100) ;
   moteur5(1800);
    delay_nms(100);
  moteur14(1800);
  delay_nms(100);
 
 moteur3(1850);
 moteur18(1600);
 moteur12(900);
 moteur9(1000);
 moteur15(1400);
 moteur6(700);
  }
   else if (c=='B')
   {
    moteur2(1550);
  delay_nms(100);
  moteur17(1500);
  delay_nms(100) ;
 moteur3(1650);
 delay_nms(100) ;
 moteur18(1700);
  delay_nms(100) ;
  moteur2(1750);
delay_nms(100);
  moteur17(1200);
  
  
 delay_nms(100) ;
  moteur8(1200);
  delay_nms(100);
  moteur11(1600);
   delay_nms(100) ;
 moteur12(1200);
 delay_nms(100);
 moteur9(700);
 delay_nms(100);
  moteur8(1500);
    delay_nms(100);
   moteur11(1300);
   
 
 delay_nms(100) ;
  moteur5(1500);
delay_nms(100);
  moteur14(2100);
  delay_nms(100);
 moteur15(1800);
 delay_nms(100) ;
 moteur6(300);
 delay_nms(100) ;
   moteur5(1800);
    delay_nms(100);
  moteur14(1800);
  delay_nms(100);
 
 moteur3(1850);
 moteur18(1600);
 moteur12(900);
 moteur9(1000);
 moteur15(1400);
 moteur6(700);}
  }
  




/*----------Dans Le Fichier stm32f4xx_it on ajoute----------------
extern char c;
extern __IO uint8_t cursor;
extern __IO char buffer[64],result[64];
void USART3_IRQHandler(void){


    c= (char)USART_ReceiveData( USART3);
usart_receive(c);} */
//------------------Dans Le fichier Main----------------------------
 //usart_lowLevelInit()
//if (flag==0) flag=1;
//#include "usart_config.h"  

Attachments

Outcomes