AnsweredAssumed Answered

Can't set/reset a bit

Question asked by perun.raphael on May 4, 2015
Latest reply on May 4, 2015 by Clive One
Hello everyone.
My target is STM32F091C I want to send something using SPI and after that make an impulse with a bit of my microcontroller. On my scope I see that I send well the data but the impulse is not generate.

Here is the code of the gpio init + the function that should generate the impulse :


void init_system_gpio (void)
{
    GPIO_InitTypeDef GPIOA_Init;
    GPIO_InitTypeDef GPIOB_Init;
    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA | RCC_AHBPeriph_GPIOB,ENABLE); /*PORT B and PORT A are used*/
    /*PORT B Configuration*/
    GPIOB_Init.GPIO_Pin =GPIO_Pin_3 | GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7 | GPIO_Pin_13 | GPIO_Pin_15;
  GPIOB_Init.GPIO_Speed = GPIO_Speed_50MHz;
  GPIOB_Init.GPIO_Mode = GPIO_Mode_AF;
  GPIOB_Init.GPIO_PuPd = GPIO_PuPd_NOPULL;
  GPIOB_Init.GPIO_OType = GPIO_OType_PP;
  GPIO_Init(GPIOB, &GPIOB_Init);
    
    GPIO_PinAFConfig(GPIOB, GPIO_PinSource3, GPIO_Mode_OUT); //Freq_UPD
    GPIO_PinAFConfig(GPIOB, GPIO_PinSource4, GPIO_Mode_OUT); //LED Debug 1
    GPIO_PinAFConfig(GPIOB, GPIO_PinSource5, GPIO_Mode_OUT); //LED Debug 2
    GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_Mode_IN);  //BP1
    GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_Mode_IN);  //BP2
    GPIO_PinAFConfig(GPIOB, GPIO_PinSource13, GPIO_AF_0);    //SPI2 CLK
    GPIO_PinAFConfig(GPIOB, GPIO_PinSource15, GPIO_AF_0);    //SPI2 MOSI
    
    /*PORT A Configuration*/
    GPIOA_Init.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_4 | GPIO_Pin_9| GPIO_Pin_10 | GPIO_Pin_15;
  GPIOA_Init.GPIO_Speed = GPIO_Speed_50MHz;
  GPIOA_Init.GPIO_Mode = GPIO_Mode_AF;
  GPIOA_Init.GPIO_PuPd = GPIO_PuPd_NOPULL;
  GPIOA_Init.GPIO_OType = GPIO_OType_PP;
  GPIO_Init(GPIOA, &GPIOA_Init);
 
    GPIO_PinAFConfig(GPIOA, GPIO_PinSource0, GPIO_Mode_AN); //ADC_IN0
    GPIO_PinAFConfig(GPIOA, GPIO_PinSource4, GPIO_Mode_AN); //DAC_OUT1
    GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_0);        //UART1 TX
    GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_0);        //UART1_RX
    GPIO_PinAFConfig(GPIOA, GPIO_PinSource15, GPIO_Mode_OUT);//RST DDS
}



void freq_ud_dds(void){
    GPIOB->ODR=(GPIOB->ODR)|0x04;
//    int i =0;
//    GPIO_WriteBit(GPIOB, GPIO_Pin_3, Bit_SET);
//    while(i<200) i++;
//    GPIO_WriteBit(GPIOB, GPIO_Pin_3, Bit_RESET);
//    GPIO_SetBits(GPIOB, GPIO_Pin_3);
//    GPIO_ResetBits(GPIOB, GPIO_Pin_3);    
};

As you can see in this last function I tried many ways to set/reset my bit...
If you can help me to generate this pulse, it would be great !
Thank you

Outcomes