AnsweredAssumed Answered

With STM32F429I-DISCO Along side of "IS42S16400J SDRAM" Connecting another FMC Device?

Question asked by mn.bharadwaj on Apr 27, 2015
Dear All,
Is it Possible to Connect another FMC device along side of IS42S16400J in STM32F429I-DISCO
board, does the Address line and Data line causes any problem to the other FMC device from the onboard SD RAM(IS42S16400J )


Note: External device Voltage is same as the SDRAM Voltage level, Control lines are different for the External interfacing device,Except Data and the Address bus are shared Between SDRAM and the External FMC device.


Thanks for your valuable response, in advance.

Outcomes