AnsweredAssumed Answered

STEVAL-MKI109V2 with STEVAL-MKI142V1 - I2C mode

Question asked by anderson.todd on Jul 29, 2015
Latest reply on Jul 31, 2015 by Licciardello.Antonel
All:
I have procurred a STEVAL-MKI109V2 and plug-in board STEVAL-MKI142V1 (LPS25H). 

When I bring up the UNICO "Cross-platform User Interface for MEMS demonstration kits", I am able to see that the device is operating, and it has good values. However, can the interface be changed from the default SPI to run as I2C?

I would like to do this to evaluate a target board that has been made up with an I2C interface.

I realize that I2C may not be an option for the demo, but is it an option?
If so, how do I change the UNICO settings to use the I2C option?

Regards,
Todd Anderson

Outcomes