AnsweredAssumed Answered

PWM max voltage 3 V !!!

Question asked by claude.antoine on Feb 18, 2015
Latest reply on Feb 18, 2015 by Clive One
I use a STM32f4vgt6 and I configured the PWM to control a DC motor. The problem is that when I measure the output PWM tention I notice that it does not exceed the 3V. When I connect the VDD pin to 5V, the problem is solved and the max output be came 5V ! Who can explain me this phenomenon ? thank you in advence 

Outcomes