AnsweredAssumed Answered

Timer 2 PWM Mode Available?

Question asked by roofie01 on Jan 27, 2015
Latest reply on Jan 27, 2015 by Clive One
Hello,

I am testing an application on a Discovery STM32F4 board (MMB997C)

I need a counter for very low frequency generation: 5Hz to 100Hz, so it looks like Timer 2 is the only one that will work OK to do the job as it's the only 32 bit timer (someone can stop me anytime if that is not correct)

I've tried setting up Timer 2 with PWM and it does not appear to work. Will PWM1 and/or PWM2 work OK with any of the Timers? Can someone point me to an example?

Thank you.

Outcomes