AnsweredAssumed Answered

Start program from Flash when power on. (Discovery stm32f407)

Question asked by pereira.patrick on Dec 7, 2014
Latest reply on Dec 8, 2014 by Clive One

When I program the discovery board with openocd and reset the board I can see the program running.
But when I turn off the board I need to connect with the openocd to run the program.

I Dont know why I need to use the command 'reset' of the openocd to run the code if the program is in the flash and on the address 0x0800.0000.

Outcomes