AnsweredAssumed Answered

Does the STM32F429 work with Discover-MO DM-STF4BB?

Question asked by Barta.Hank on Nov 24, 2014
Latest reply on Nov 25, 2014 by Clive One
I'm new around here and still not sure where all of the information I seek can be found. Any help is most appreciated!

That would be (AFAIK) MBMB1075 B-01 and DM-STF4BB if those are more meaningful designations.

I have these (along with camera and LCD that come with the Base Board.) It is not obvious to me that the processor board is meant to work with this base board since the processor has two 64 pin headers and the Base Board has two 50 pin (hole?) sockets. At the least, I would need to know how to orient and align the processor board with the base and I have not found anything on that in a quick scan of the manual for either of these.

I did find a picture of the STM32F4DISCOVERY  processor board that seems to be the one intended for that base board. Comparing pinouts shows ground pins on one have other functions on the other which tells me they are incompatible. 

Is that the case or am I missing some information?

Thanks!
Hank

Outcomes